DB problem of 2874

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DB problem of 2874

1,372 Views
1318910567
Contributor I

微信图片_20191229130440.jpgBGA2874Adjust to the voltage of 2.5V, 18 mA is almost 10 DB worse.

The two tubes on the graph add up to noise, right?

0 Kudos
Reply
1 Reply

1,264 Views
LPP
NXP Employee
NXP Employee

This noise calculation is not correct. The noise contribution of the second stage amplifier is divided by the second stage gain.

Please, see NF calculation formula in this document:
https://www.nxp.com/docs/en/white-paper/RFLNAWP.pdf

NFsys = 0.5dB + 3.5dB@G=30dB = 0.505dB

Have a great day,

Pavel
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply