Can P3S0200GM be used for USB FS signals?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can P3S0200GM be used for USB FS signals?

Jump to solution
2,851 Views
mhavu
Contributor I

Can P3S0200GM be used for multiplexing full-speed USB signals? We already use it elsewhere in the design, so it would be convenient to use the same part, if possible.

0 Kudos
Reply
1 Solution
2,837 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear M. Havu,

the P3S0200GM is a 2-bit bidirectional voltage-level translator and multiplexer designed primarily for I²C and I³C signals. It is not suitable for multiplexing full-speed USB signals.

It does not support the USB differential signaling (D+/D-).

We can recommend you CBTL02043A; CBTL02043B 2:1 mux/demux for the USB signals. 

https://www.nxp.com/products/interfaces/usb-interfaces/3-3-v-two-differential-channel-2-1-multiplexe...

With Best Regards,

Jozef

View solution in original post

0 Kudos
Reply
1 Reply
2,838 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear M. Havu,

the P3S0200GM is a 2-bit bidirectional voltage-level translator and multiplexer designed primarily for I²C and I³C signals. It is not suitable for multiplexing full-speed USB signals.

It does not support the USB differential signaling (D+/D-).

We can recommend you CBTL02043A; CBTL02043B 2:1 mux/demux for the USB signals. 

https://www.nxp.com/products/interfaces/usb-interfaces/3-3-v-two-differential-channel-2-1-multiplexe...

With Best Regards,

Jozef

0 Kudos
Reply