CWH-UTP-ONCE-HE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CWH-UTP-ONCE-HE

2,888件の閲覧回数
Abdulkerim
Contributor I

I need support device list of CWH-UTP-ONCE-HE programmer
or can you sent me the software by Email
I need to writing and reading these CPU
56F8006, 56F8023, 56F8034 etc...

I will buy this programmer or any other programmer that will help me in my work
Is shipping to Turkey available?

Email: [email protected]

thank you so mutch

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,871件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As it's designation 56800E Flash Programmer implies that the tools just writes code/data to flash instead of reading it to a flash, furthermore, reading flash to a file may infringe the code IP, so it is not a main function. I think the CodeWarrior for MCU tools provides the function.

Click the "Add Action", there is "Dump Flash" option, you can download memory to file with the option.

Hope it can help you

BR

Xiangjun Rong

 

xiangjun_rong_0-1619491653102.png

 

0 件の賞賛
返信

2,874件の閲覧回数
Abdulkerim
Contributor I

No problem for a computer system
Because my computer is running on Windows 7 64 bits mainly
But I didn't see that the software had a "reading" icon.
I need to write and read memory for that controller

MC56F8006, 13, 23, 34 and MC56F82746V
Can you advise me
thank you
0 件の賞賛
返信

2,877件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Abdulkerim,

Pls go to the link:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

 

and download the