Our main question concerns the behavior of the vehicle when an emergency alert is received from DAB while another media source is active, such as Spotify via Bluetooth/CarPlay/Android Auto or an FM radio station.
Specifically, we would appreciate your technical clarification on the following points:
Automatic Source Switching: When an ASA emergency alert is received over DAB while the user is listening to FM radio or Spotify, how does the system automatically switch to the DAB emergency announcement and display the relevant alert information?
System Responsibility: Which component is responsible for this behavior? Is the alert detection and triggering handled by the ASA chip itself, or does the DAB receiver/head unit need a control interface that allows it to interrupt the currently active media source and switch to DAB audio?
Vehicle Integration: Does the DAB receiver directly control the audio source and display, or does it send an alert notification or trigger signal to the vehicle's infotainment system, which then performs the source switching and displays the alert?
Standards and Implementation: Does the relevant ASA/DAB standard define this behavior and the required interface between the receiver and the vehicle infotainment system, or are these implementation details left to the receiver manufacturer and vehicle OEM?
Technical Requirements: Are there any specific hardware interfaces, software APIs, control signals, or infotainment integration requirements necessary to ensure that an emergency alert can override the currently active media source?
Our objective is to understand whether this functionality is primarily provided by the ASA receiver/decoder or whether additional integration with the vehicle's infotainment system is required.
Any relevant technical documentation, system architecture diagrams, or implementation guidelines would be greatly appreciated.