ADC for MC56F83783

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC for MC56F83783

2,295 Views
Mariya
Contributor I

I am using MC56F83783 controller.As the controller does not support processor expert.I want an idea  for Single ended sequential ADC with  LOOPING scan mode..

0 Kudos
Reply
3 Replies

2,261 Views
Mariya
Contributor I

Can you provide an application note for mc56f83783 controller, will be helpful going forward.

0 Kudos
Reply

2,254 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

 

For the application note of MC56F83xxx, pls download from the website:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

Hope it is helpful

BR

XiangJun Rong

0 Kudos
Reply

2,265 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The PE(Processor Expert) is no longer supported for the MC56F83xxx family, you have to use SDK package which is run on CodeWarrior for MCU ver11.x.

Pls download SDK package from the link:

https://mcuxpresso.nxp.com/en/welcome

 

In the SDK example, there is ADC example, pls try to test it, if you require the looping ADC mode, I suppose you have to modify the ADC example code.

Hope it is helpful

BR

XiangJun Rong

0 Kudos
Reply