simple assembly "illegal instruction" exception handler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

simple assembly "illegal instruction" exception handler

3,357件の閲覧回数
order324
Contributor I

Any one have a simple assembly "illegal instruction" exception handler that allows the program to continue after skipping over the illegal instruction?  Here is what I have so far (it executes the routine but the routine doesn't work):

 

 DEBUG_EXC_HANDLER:
        
        move.l #0x00000001,%D0 || put 1 in D0
        add.l %D0,%D3          || add D0 to D3 and put the result in D3

                                      ||(simple counter so I can see what's happening)       
        nop
        nop
        
        move.l (%A7)+,%D7  || pop status off stack
        move.l (%A7)+,%D7  || pop pc off stack

      
        move.l #0x00000002,%D1
        move.l %D7,%D0
        add.l %D1,%D0          || add D1 to D0 and put the result in D0
        move.l %D0,-(%A7)      || set top of stack to be error pc+2
        
        nop
        nop
        
        rte
        
        nop
        nop

 

|| end

 

 

With this handler, I get a "format error" exception (different exception) right after the rte.  Clearly I am not manipulating the stack correctly.  Any ideas?  Is it even possible to recover?

 

Thanks,

 

Niel

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,029件の閲覧回数
taigbr
Contributor I

Hi Niel,

since you try to return with a RTE the processor expects to find

a format field on the stack. You probably intended to return with

a RTS instruction. Take a look into the documentation about

"Exception Stack Frame Definition".

Regards, Georg

0 件の賞賛
返信

2,029件の閲覧回数
order324
Contributor I

Ok that seemed to fix it.  I had read the section about the two entries on the stack but it was not clear to me that the rte read back that info and used it.

 

Thanks,

 

Niel

0 件の賞賛
返信