Where can I discuss MPC8260

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I discuss MPC8260

4,805件の閲覧回数
dorjee
Contributor I
hello,
where can i discuss issues related to MPC8260,
 
here is my question
what is the criteria for putting the buffer in external memory (fcc ethernet),
can i create buffer in any part of the external RAM, or there r some conditions to
be taken care of.
thnx
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,093件の閲覧回数
dorjee
Contributor I
hey arroju,
 
my previous answer is not with respect to your question,that is very evident from the answer,FCC is independent from MCC,
 
Actually i was replying to myfirst post,as i got the answer to my post, i thought of sharing it in the forum for those who  visits the thread.
 
I am not much aware of MCC though but what i found is that your question is not very clear.take this as suggestion..
 
post in following manner
       1.what your intentions are or say what you want to do
        2.and then specify what you get ,
 
so that whoever sees your post can answer you in better way.
 
if u need answer urgently then u may write to freescale support
they are always ready to answer our question however silly it may be.
 
regards
dk
0 件の賞賛
返信

2,093件の閲覧回数
dorjee
Contributor I
You can place FCC buffer descriptors (BDs) and the buffers anywhere in
external memory. Please note that the FCC uses burst transactions to
access memory, therefore your SDRAM must be properly programmed to
support burst operations.

Please be aware, the DPRAM memory doesn't support burst operations,
therefore it can not be used to store FCC buffer descriptors and buffers.

0 件の賞賛
返信

2,093件の閲覧回数
arroju
Contributor I
Is your explanation related to my issue?
 
If yes what is the relation between MCC and FCC?
 
Iam using MCC in Transparent mode.
 
 
0 件の賞賛
返信

2,093件の閲覧回数
arroju
Contributor I
Hi
 
Iam facing problem with MCC Transparent mode.
After every BD I transmit ,FF are getting padded at the end of the buffer,the number of FF are equal to the number of time slots programed.
Iam not setting Last bit in my BD.
 
Any one can help on this issue.
 
Thanks,
Vijay
 
0 件の賞賛
返信