What is the dif between MCF5253 and MCF5251?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the dif between MCF5253 and MCF5251?

1,471 Views
tkrajewski
Contributor I

What is the dif between MCF5253 and MCF5251? If we have been using the 5253 can we switch to the 5251?

Thank you

0 Kudos
Reply
1 Reply

1,339 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

MCF5253 has the same modules with MCF5251.
The differences between two chips is that:
The MCF5251 which comes with license access to a variety of MP3 encode and decoders and the MCF5253 which is a cheaper version that doesn't come with audio software licenses.

MCF5253 is pin to pin compatible with MCF5251.

best regards,

Mike

0 Kudos
Reply