USB Printer Device driver and IEEE Device ID string

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Printer Device driver and IEEE Device ID string

2,044件の閲覧回数
mattlang
Contributor I

I have an MCF51JE256CLK that I made a printer device. It enumerates as a printing device and loads the standard kernal mode driver for printing on windows. USBPrint.sys. I can print to it by using the "Add Printer" Wizard for windows and open a USB001 port. But my device still lives in the unspecified category in "Devices and Printers".

 

What I would like to do is use an existing .dll user mode driver with a custom .inf and .GPD file. To my understanding, windows checks all the .inf files when a device is plugged in and finds the one with the best "rank". Would I be able to write an .inf file that makes windows pick my .inf file as the best one, and have the file point to an existing printer .dll and a custom .GPD? For example the generic text only driver or some PCL6 driver

 

My other question is: The PC never asks for my Device ID string that describes my printers capabilities such as manufacturer and PCL. When is the PC supposed to ask for this?

 

  1. uint_8 printer_device_id[PRINTER_DEVICE_ID_STRING_SIZE] =  
  2. {  
  3.  
  4.      0x00,0x42,      // Length of the Device ID string (MSB/LSB) including the 
  5.     'M',            // two length bytes 
  6.     'A', 
  7.     'N', 
  8.     'U', 
  9.     'F', 
  10.     'A', 
  11.     'C', 
  12.     'T', 
  13.     'U', 
  14.     'R', 
  15.     'E', 
  16.     'R', 
  17.     ':', 
  18.     'X', 
  19.     'X', 
  20.     'X', 
  21.     'X', 
  22.     'X', 
  23.     'X', 
  24.     ';', 
  25.     'M', 
  26.     'O', 
  27.     'D', 
  28.     'E', 
  29.     'L', 
  30.     ':', 
  31.     'P', 
  32.     'T', 
  33.     'I', 
  34.     '-', 
  35.     'P', 
  36.     'R', 
  37.     '0', 
  38.     '0', 
  39.     '1', 
  40.     ';', 
  41.     'C', 
  42.     'O', 
  43.     'M', 
  44.     'M', 
  45.     'A', 
  46.     'N', 
  47.     'D', 
  48.     ' ', 
  49.     'S', 
  50.     'E', 
  51.     'T', 
  52.     ':', 
  53.     'P', 
  54.     'C', 
  55.     'L', 
  56.     '5', 
  57.     ';', 
  58.     'C', 
  59.     'L', 
  60.     'S', 
  61.     ':', 
  62.     'P', 
  63.     'R', 
  64.     'I', 
  65.     'N', 
  66.     'T', 
  67.     'E', 
  68.     'R', 
  69.     ';' 
  70. }; 

 

 

Thanks

ラベル(1)
0 件の賞賛
返信
0 返答(返信)