Setting VBR on 5282

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting VBR on 5282

1,943 Views
SVC1
Contributor I
Hi,
 
I would like to keep the interrupt table into internal flash.
 
I would like my application to be at address 0x8000, how do I set up the VBR to this address (since the lower 20 bits are not implemented)?
 
Thanks,
Simon
 
Labels (1)
0 Kudos
Reply
1 Reply

1,305 Views
UK_CF_FAE
NXP Employee
NXP Employee
Hi SVC1,
 
The vector table must be located on a 1MByte boundary, and so you will not be able to place it at 0x8000. I think that you will need the vector table at 0x0000_0000.
 
Mark.
0 Kudos
Reply