SPI pins dead on a M5208EVBe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI pins dead on a M5208EVBe

2,053件の閲覧回数
order324
Contributor I

I have some assembly code software running on a M5208EVBe board and a Freescale Coldfire processor.  I am able to load the code and run it (by setting the pc to the start of the code) in both the BDM debug mode (with GDB debugger), and by using the dBUG terminal program loaded into the ram of the processor during default startup.  However, despite running all my QSPI setup commands (which wiggle the pins in simulation), no SPI activity occurs on the pins at all.  CSB is stuck low, while the QCLK is also stuck low.

 

For reference, here is a list of all the registers I set:

 

0xA102 into QMR

0x0100 into QIR

0x01 into ICR31

0x0400 into QDLYR

0x0020 into QAR

0x8e00 into QDR (5 times, autoinc each time)

0x0000 into QAR

(various data) into QDR

0x1400 into QWR

0x8400 into QDLYR to start!

 

and nothing happens.  The interrupt does work, but it hoses the program because I don't know how to set the interrupt vector table using dBUG.

 

I have searched the forum and the FAQs for answers to this question and I have not seen one.

 

Thanks!

 

Niel

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,397件の閲覧回数
RichTestardi
Senior Contributor II

Did you remember to set the QSPI Pin Assignment Register (PAR_QSPI) to set those pins to their primary (QSPI) functions (as opposed to the default GPIO functions)?

 

-- Rich

 

PS See reference manual section 13.3.5.5.

Message Edited by Rich T on 2009-02-24 03:00 PM
0 件の賞賛
返信

1,397件の閲覧回数
order324
Contributor I

Well it looks like I did forget to set the PAR_QSPI bits correctly.  I went back and set those bits correctly as well as the PAR_UART bits.  However, I still don't see any wiggling of the spi signals on the eval board, except the qspi_clk (labeled QCLK) is now high.

 

Any more ideas?  This has really got me stumped.

 

Thanks,

 

Niel

 

0 件の賞賛
返信