SD-Card interface for MCF52259 using QSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD-Card interface for MCF52259 using QSPI

4,304 Views
sven_kaemmer
Contributor III
Hello,

 

I'm looking for a schematic and/or a code example for using the qspi of MCF52259 to interface a sd-card. Can everyone helps me?

Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

2,178 Views
PetrL
NXP Employee
NXP Employee

Hi,

 

sd card driver is part of MQX 3.5 release (mfs/examples/sdcard + driver is under mqx/source/io/sdcard). You would find examples for the EVBs with SDCARD slot (twr-mcf52259 + twr-mem extension board, twr-mcf51cn +twr-mem extension board, m52277evb)

 

PetrL

 

 

 

0 Kudos
Reply

2,178 Views
mjbcswitzerland
Specialist V

Hi

 

http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF

 

Regards

 

Mark

 

 

www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

 

 

0 Kudos
Reply