Reset on watch dog timer expires

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reset on watch dog timer expires

ソリューションへジャンプ
7,695件の閲覧回数
MCF52233
Contributor III

Hi all,
I hv MCF52233DEMO board in which i want to use watch dog timer to reset the program after watch
dog timer expires.
/******* from main.c ********************/
MCF_INTC0_IMRL &= ~( MCF_INTC_IPRL_INT8 | 1 ); // Enable Irq 8 (bit 0 should allways be 0)

MCF_INTC0_ICR07=MCF_INTC_ICR_IL(4);

MCF_SCM_CWCR = MCF_SCM_CWCR_CWE | // Enable WDT
//MCF_SCM_CWCR_CWT(1) | // 2^19 bus cycles.
MCF_SCM_CWCR_CWT_2_23 |
MCF_SCM_CWCR_CWTA | // Enable Transfer Ack.
MCF_SCM_CWCR_CWTAVAL ;

/************** exception.c *************/

__interrupt__ void wdtISR( void )
{

MCF_SCM_CWCR |=MCF_SCM_CWCR_CWTAVAL |MCF_SCM_CWCR_CWTIF ;
MCF_RCM_RCR |= MCF_RCM_RCR_SOFTRST; // Set software reset request bit.
}

and also add entry in vetor table at 72 i.e. 64+8

but rather than program reset program stop executing.
Is i miss something or any flaw to set the values??
Plz help me out.
ラベル(1)
0 件の賞賛
返信
1 解決策
5,026件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

Here is code to configure a 2s watchdog timeout

 

CWCR = (CWE | WATCHDOG_2_SEC | CWTA | CWTAVA | CWTIF);

fnSetIntHandler(SW_WD_VECTOR, (unsigned char *)_sw_wdog_timeout);

IC_ICR_0_8 = (INTERRUPT_LEVEL_7 | INTERRUPT_PRIORITY_7);

IC_IMRL_0 &= ~(SW_WDG_PIF_INT_L | MASK_ALL_INT);

 

The handling routine is 

 

static __interrupt__ void _sw_wdog_timeout(void)
{
    RESET_RCR = SOFT_RST;                                                // command a soft reset of the board
}

 

Note that the watchdog should best be given highest (NMI) priority so that it can fire when another interrupt routine fail.

It is however not fool-proof since it relies on the watchdog interrupt handler being able to run (which is not 100% guarantied) - see http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=1051&query.id=148409#... 

 

The Backup Watchdog Timer in other V2 MCU parts (like Kirin3) is much improved. See http://www.utasker.com/forum/index.php?topic=505.0

 

Regards

 

Mark

 

www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

 

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
5,026件の閲覧回数
terryt
Contributor I

I'm running the InterNiche stack using the M52233Demo board also.

 

Same issue here. It doesn't work!!!!!!!!! 

 

/**Int_handlers.c **/

 

__interrupt__ void wdtISR( void )
{

MCF_SCM_CWCR |=MCF_SCM_CWCR_CWTAVAL |MCF_SCM_CWCR_CWTIF ;
MCF_RCM_RCR |= MCF_RCM_RCR_SOFTRST; // Set software reset request bit.
}

/**Int_handlers.c **/

 

MCF_INTC0_ICR07=MCF_INTC_ICR_IL(7); //highest priority.
 

MCF_INTC0_IMRL &= ~( MCF_INTC_IMRL_INT_MASK1); //Using one other Interrupt. 
MCF_INTC0_IMRL &= ~( MCF_INTC_IMRL_INT_MASK7); //Watchdog Interrupt. 


MCF_SCM_CWCR = MCF_SCM_CWCR_CWE | // Enable WDT
MCF_SCM_CWCR_CWT_2_23 |
MCF_SCM_CWCR_CWTA | // Enable Transfer Ack.
MCF_SCM_CWCR_CWTAVAL ;

/***MCF52235_vectors.s**

 

vector48   .long _wdtISR

 

 

It never causes an interrupt at this vector. 

 

The link says issued resolved. I say it isn't. Can anyone clear this up?

 

Thanks,

Terry

0 件の賞賛
返信
5,026件の閲覧回数
MCF52233
Contributor III

Hi terry,

just replace this line

 

MCF_INTC0_ICR07=MCF_INTC_ICR_IL(7); //highest priority.

 

to

MCF_INTC0_ICR08=MCF_INTC_ICR_IL(7); //highest priority.

 

0 件の賞賛
返信
5,026件の閲覧回数
terryt
Contributor I

Hey Abhijit,

 

Thanks for the quick reply. It gave me some focus on what to look for.

 

The only reference to Control registers concerning the Watchdog was the one below.  

It wasn't very clear in this data sheet. 

 

From the Data Sheet MCF52235RM.pdf Section 13-10..

 

CWRI

Core watchdog interrupt select.

0 If a time-out occurs, the CWT generates an interrupt to the processor core. The interrupt level for the CWT is

programmed in the interrupt control register 7 (ICR7) of INTC0.

 

 

Same code from me before but I hardcoded the ICR08 = 0x3F;

 

 

Here is what worked for me.......

 


MCF_SCM_CWCR = MCF_SCM_CWCR_CWE

| // Enable WDT
MCF_SCM_CWCR_CWT_2_23 |
MCF_SCM_CWCR_CWTA | // Enable Transfer Ack.
MCF_SCM_CWCR_CWTAVAL ;

MCF_INTC0_ICR08 |= 0x3F; //highest priority. 

MCF_INTC0_IMRL &= ~( MCF_INTC_IMRL_INT_MASK8); //Watchdog Interrupt. 
 

 

 

 

 

 

 

0 件の賞賛
返信
5,026件の閲覧回数
terryt
Contributor I

I was trying to fix the last couple lines. I hit the tab key which sent before I wanted to.......

 

Here is a cleaned up version......... 

 

MCF_SCM_CWCR = MCF_SCM_CWCR_CWE

                          | MCF_SCM_CWCR_CWT_2_23

                          | MCF_SCM_CWCR_CWTA

                          | MCF_SCM_CWCR_CWTAVAL

                          | MCF_SCM_CWCR_CWTIF;

MCF_INTC0_ICR08 |= 0x3F; //highest priority. 

MCF_INTC0_IMRL &= ~( MCF_INTC_IMRL_INT_MASK8); //Watchdog Interrupt.

MCF_INTC0_IMRL &= ~( MCF_INTC_IMRL_MASKALL); //Enable.

 

Thanks again Abhijit.......

 

 

0 件の賞賛
返信
5,026件の閲覧回数
MCF52233
Contributor III

Hi terry,

    The configuration is looking fine but might be still remains something.

I'm not a expert but still i can give some ways to approch d task.

U can try without InterNiche.just create new project which include this

watch dog releted configuration.

Finally 1 question is remains dat how u test it???

In my case i made a basic timer who clear the releted register

 

MCF_SCM_CWSR = 0x55;
MCF_SCM_CWSR = 0xAA;

 

when i commented dat part i.e not clearing this then ISR is callled from vector48. 

 

0 件の賞賛
返信
5,026件の閲覧回数
terryt
Contributor I

Hey Abhijit,

 

What helped me out the most was using a baseline Processor Expert project with having only a watchdog (no Internice). This showed me the correct values for all registers and vectors. The datasheet was just not clear enough.

 

I tested by setting a breakpoint at the interrupt vector routine and not writing the 0x55 & 0xAA to the CWSR.

 

It took about 20 seconds for the interrupt to engage. It works!

 

Thanks again,

TT

0 件の賞賛
返信
5,027件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

Here is code to configure a 2s watchdog timeout

 

CWCR = (CWE | WATCHDOG_2_SEC | CWTA | CWTAVA | CWTIF);

fnSetIntHandler(SW_WD_VECTOR, (unsigned char *)_sw_wdog_timeout);

IC_ICR_0_8 = (INTERRUPT_LEVEL_7 | INTERRUPT_PRIORITY_7);

IC_IMRL_0 &= ~(SW_WDG_PIF_INT_L | MASK_ALL_INT);

 

The handling routine is 

 

static __interrupt__ void _sw_wdog_timeout(void)
{
    RESET_RCR = SOFT_RST;                                                // command a soft reset of the board
}

 

Note that the watchdog should best be given highest (NMI) priority so that it can fire when another interrupt routine fail.

It is however not fool-proof since it relies on the watchdog interrupt handler being able to run (which is not 100% guarantied) - see http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=1051&query.id=148409#... 

 

The Backup Watchdog Timer in other V2 MCU parts (like Kirin3) is much improved. See http://www.utasker.com/forum/index.php?topic=505.0

 

Regards

 

Mark

 

www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

 

0 件の賞賛
返信
5,026件の閲覧回数
MCF52233
Contributor III
Thanks.
I also read given link by u n it is really very helpful.
Now i hv working watch dog time out reset.Only my mistake was i use ICR7 rather than ICR8.
When CWT = 0 i.e. for 2^9 bus cycles then how much actually time is mean for operating on 60Mhz???

Thanks once again for ur valuable time for the entire forum.
0 件の賞賛
返信