Reset Vector for MCF5445x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reset Vector for MCF5445x

2,608件の閲覧回数
Thad
Contributor III
I am writing a boot loader for an MCF5445x based target.  I am wondering if it is possible to issue a soft reset but then have the reset vector route execution to the kernel I have just loaded into RAM (i.e. base address at 0x4002000) rather than do its usual load from ROM (0x00000000) or via SPI.  I've been reading the MCF54455RM spec doc and my first impression is that it is not easily done, but perhaps I missed something.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,763件の閲覧回数
Thad
Contributor III
I thought as much.  I was hoping for a shortcut, but it looks like I'll just have to set the board state manually before jumping to the kernel entry point.  Thanks.

0 件の賞賛
返信

1,763件の閲覧回数
kmahan
Contributor I
I don't think you can.  You either boot off a flexbus device or using the Serial Boot Flash (SBF) over SPI.

The two signals that control booting are BOOTMOD[1:0] (section 10.2.1 in the RM).  Your options are:
  • Boot from Flexbus with defaults
  • Boot from Flexbus and override defaults via data bus
  • Boot from Flexbus and override defaults via the serial boot facility
  • Reserved (just for those wondering about the last bit combination)
You can't go directly to SDRAM.  Also you'd need to setup the SDRAM controller before you could execute code from it.

--Kurt
0 件の賞賛
返信