RTC registers dont function if SuperCap drained? (MCF52210)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC registers dont function if SuperCap drained? (MCF52210)

1,964 Views
junkers13
Contributor I
Hi, I'm using the M52210DEMO board and the RTC in the processor runs fine, but when the board hasn't been powered in a long time and then is powered the RTC clock just doesnt work.  Values can't even be written to the registers.  The only thing I can think of is that it has to wait for the Supercap to charge.  Because after active for I donno 10 mins the clock begins to run again.
 
Anyone know how to prevent this?
 
Thanks


Message Edited by joey c on 2008-08-13 09:38 AM
Labels (1)
0 Kudos
Reply
1 Reply

1,268 Views
junkers13
Contributor I
yea I just discharged the SuperCap and ran the debug to look at the registers and they are not changing and can not be written to.  So when the Supercap is drained it is causing the RTC to stop functioning.  Anyone know how to get around this?
 
Thanks


Message Edited by joey c on 2008-08-13 01:03 PM
0 Kudos
Reply