Quick way to start using a Coldfire and USB CDC !?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Quick way to start using a Coldfire and USB CDC !?

3,723 Views
Claude_Sylvain
Contributor I
Hello all,
 
With the HC08 JW32 MCU, there is an Application Note (AN3153) that make easy to start using USB CDC (Virtual Serial COM port) with that processor.
 
Is there any similar resource for the Coldfire MCU, like the MCF52221 ?
I search a lot, and do not found anything  :smileysad:
 
 
Claude.
 
Labels (1)
0 Kudos
Reply
3 Replies

1,691 Views
JWW
Contributor V
Claude,
 
Sorry it is so hard to find.  The CDC example code, with full project, is available on the Coldfire pages.
It is included in the CMX_Lite code. 
 
 
There is also a new low end Coldfire part with integrated USB.. It was just announced yesterday.
 
Please see these this link:
 
The CMX_Lite stack is also available for this new part.
 
Hope this helps!
 
-JWW
 
 
0 Kudos
Reply

1,691 Views
Claude_Sylvain
Contributor I
JWW,
 
Thank you for your help.
 
Claude.
 
0 Kudos
Reply

1,691 Views
JWW
Contributor V
Claude,
 
Your welcome... I hope you enjoy.  Let us know if we can help more.
 
One more link for everybody reading this thread... We announced two new products for USB yesterday...
And created a web site to help you navigate the numerous product offerings.
 
Weblink is:
 
 
 
-JWW
0 Kudos
Reply