Place MC68332 in high impedance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Place MC68332 in high impedance

2,290 次查看
chriscrde
Contributor I
Hello,
I'm developping a board test in boundary scan and i need to place an MC68332 in high impedance in order to test adress and data bus of the board.
I think that i have to use the TSC pin but I don't know how to use it. The document M68331/332TUT/D says that :

Driving this pin to approximately 1.6 times causes the MCU to place all output drivers in a high-impedance state, isolating the MCU from the rest of the system.

But it doesn't work.

Can you say me how to do ?

Thanks

 

标签 (1)
0 项奖励
回复
1 回复

1,031 次查看
macl
Senior Contributor I
Hi,
 The TSC signal must remain asserted (1.6*VDD) for approximately ten clock cycles in order for drivers to change state.  This is 8V for 5V VDD.  Just don't go over 9V.
 
Thanks,
Mac
0 项奖励
回复