PEMicroProtocolPlugin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PEMicroProtocolPlugin

2,653 Views
hellamasta
Contributor I
Hi!!!
I'd like to know where to download PEMicroProtocol Plugin.

Thank you.

Alessio
Labels (1)
0 Kudos
Reply
2 Replies

1,460 Views
CompilerGuru
NXP Employee
NXP Employee
The P&E Protocol Plugin is the adapter used by the CodeWarrior IDE to talk to the P&E adapters.
It is a part of the CodeWarrior for CF installation (CW for CF 6.3) and cannot be downloaded separately.
So which version of CW are you using?
Why do you want to download the PP separately?
Are you sure you do not have it?
In case you already have it without noticing, you can configure it from within the CW ide:
Edit->Preferences->Debugger->Remote Connections
-> click add (or change while selecting an existing one)
-> select ColdFire PEMicro in the Debugger combo box.

Daniel

0 Kudos
Reply

1,460 Views
mccPaul
Contributor I
Hi
 
Try the P&E website for all things P&E:
 
 
Cheers,
 
Paul.
0 Kudos
Reply