Need help with LTIB for M5227evb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help with LTIB for M5227evb

1,687 Views
robetaynguyen
Contributor I

Hi everyone,

I have been trying to port the uCLinux onto the M5227 evaluation board. The host pc using Ubuntu 9.10 and I got the following error when executed the ./ltib command in terminal:


ltib cannot be run because one or more of the host packages needed
to run it are either missing or out of date.

Please install/upgrade these packages and then re-try.

Package                Minimum ver   Installed info
-------                -----------   ---------------
rpm-build              0             not installed
Died at ./ltib line 1242.


At the first time, the missing packages were even much more than that but I get them installed by using sudo apt-get install command. However, I couldn't find the rpm-build package anywhere by the same command as well as googling in internet. Anyone deal with the same problem or exprience with the rpm-build package pls help!

Thank you very much,

Quoc

Labels (1)
0 Kudos
Reply
1 Reply

1,279 Views
ihaveno
Contributor I
0 Kudos
Reply