Need help for M54451 EVB board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help for M54451 EVB board

2,008 Views
uolli
Contributor III

Hi all,

 

I have a hardware design project, mainly running the open source IPPBX - Asterisk (www.asterisk.org), the customer was required to use MCF54451, but i am afraid that cpu has no enough performance for Asterisk decode/code. 

So, if you have a M54451 EVB board on hand, could you please help me running following command and post output message here

---------------

in m54451 shell prompt

1. asterisk -cvvvvvvvvvvvvvvvvvgr

2. show translation

---------------

 

very appreciate your help :smileyhappy:

Labels (1)
0 Kudos
Reply
2 Replies

1,865 Views
JWW
Contributor V

Uolli,

 

We have a partner that has helped to implement the Asterisk code on the 5445x family.

 

Have you contacted Arcturus Networks?

 

They should be able to demonstrate that it can be done and provide services if needed.

 

I did find that we still have the lab setup PPT on the web, maybe this might help.

 

Slide 1

 

 

-JWW

 

0 Kudos
Reply

1,865 Views
uolli
Contributor III

Hi JWW,

 

Thanks for your reply, i saw that ppt file, but i can not found any information about M54451 EVB board at their website :smileysad:.

Will try to contract them directly or who has such board on hands will be easy more :smileyhappy:

 

Thanks.

0 Kudos
Reply