Need Help About MCF51EM256 Flash Programming Routines

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need Help About MCF51EM256 Flash Programming Routines

2,199 Views
Nur
Contributor I

Hi all,

 

I have a problem about flash programming for MCF51EM256. I downloaded application note by AN3942 document number and also downloaded software by AN3942SW number. And then I followed the instructions (also set my flash clock).  My erase function is running perfectly but my burst program is not. It is writing my datas to the given address but it can not jump to subroutine. Here are the burst code from AN3942SW;

 

 

/*******************************************************************************/

_Burst_Prog:
             move.l  d0,d4
             move.l  a1,a3
             move.l  a0,d2
             move.l  a0,d6

                  
             cmpi.l   #0x1FFFF,d6
             bgt.s    SEC_ROUT2
                             
             move.l  #(SpSubBurstEnd),a1
             move.l  #(SpSubBurst),a6
            
             bra     DOONSTACK2
            
SEC_ROUT2:   move.l  #(SpSubBurstEnd2),a1
             move.l  #(SpSubBurst2),a6


DOONSTACK2:  bsr     DoOnStack
                         
               cmpi.l   #0x1FFFF,d6
               bgt.s    SECOND_BLOCK2

FIRST_BLOCK2:
               move.l  a0,a1
               move.b  #(mF1STAT_FCCF + mF1STAT_FCBEF),d0            
               move.b  d0,F1STAT
               bra     JMP_STACK2
SECOND_BLOCK2:
               move.l  a0,a1
               move.b  #(mF2STAT_FCCF + mF2STAT_FCBEF),d0
               move.b  d0,F2STAT
JMP_STACK2:
              jsr     (A1)                      //The problem is here
           rts
 
/*******************************************************************************/
DoOnStack:
             move.l  A7,A2       /* save actual address SP */
DoOnStack1:
             suba.l  #2,a7      
            
             move.w  (a1),d0
             move.w  d0,(A7)
            
             cmpa.l  a6,a1       /* SELECTED #(SpSubBurst) or #(SpSub) */          
             suba.l  #2,a1
             bne.s   DoOnStack1

             move.l  A7,A0
             move.l  A2,A7
             rts

 

/*******************************************************************************/

 

What sould I do?

 

Thank you,

Nur

Labels (1)
0 Kudos
Reply
2 Replies

1,797 Views
kef
Specialist I

It is weird that _Burst_Prog is trying to launch flash command by writing one to FCBEF bit. If this attempt is accepted by flash controller, then CPU should runaway, because _Burst_Prog is probably in flash and flash is not readable while being programmed, CPU can't read opcodes etc. Writing one to FCBEF should be done only in one of Spxxxx routines, which are copied by DoOnStack routine to RAM(stack). Maybe they ware trying to clear FPVIOL and FACCERR bits? Try commenting out in _Burst_Prog

 

               move.b  d0,F1STAT
and

               move.b  d0,F2STAT
 

or replace

 

              move.b  #(mF1STAT_FCCF + mF1STAT_FCBEF),d0        

and

              move.b  #(mF2STAT_FCCF + mF2STAT_FCBEF),d0        

 

with

              move.b  #(mF1STAT_FPVIOL + mF1STAT_FACCERR),d0        

and

              move.b  #(mF2STAT_FPVIOL + mF2STAT_FACCERR),d0        

 

 

0 Kudos
Reply

1,797 Views
Nur
Contributor I

Thank you, but the problem is still remaining...

0 Kudos
Reply