Motor control using Coldfire MCF5270X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Motor control using Coldfire MCF5270X

2,743 Views
skaky
Contributor I

i am looking for a available referece design to control two motors (dual axis solar tracking system), if you have a design avaialble i would like to buy one for our project

 

please reply

Labels (1)
0 Kudos
Reply
2 Replies

2,491 Views
Blackdragon
Contributor I

Shyam,

What type of motors are you using. I have dual PMDC Tower motor cards that slave from a Tower processor card.

Found here: cLS-FSTS-MC2-5

Bill

0 Kudos
Reply

2,491 Views
RHA
Contributor II

Hey Shyam,

we dont have a reference design for dual motor control with the MCF5270X . However we do have some Reference Designs with dual motor control. This is a demo we have using Kinetis,

you can find some nice appnotes such as this one:

BLDC Motor Control with Hall Effect Sensors Using MQX on Kinetis

http://cache.freescale.com/files/32bit/doc/app_note/AN4376.pdf

so it really depens on what type of motor you are looking for... I suggest you go into Freescale's Motor Control site

http://www.freescale.com/motorcontrol

0 Kudos
Reply