METHOD "POST" on mcf5223x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

METHOD "POST" on mcf5223x

1,426 次查看
FLATER
Contributor I
Hello... I want to use method post at embedded web server. Idon't know why is not supported. I try to change rcv buffer size but doesn't work for me. Can somebody help me?
标签 (1)
0 项奖励
回复
1 回复

873 次查看
mjbcswitzerland
Specialist V

Hi

 

If you can't find a solution, take a look at the uTasker project. It supports posting files to the application or to the file system and also posting parameters. It operates with all browsers, as well as cURL. It also supports posting new (optionally encrypted) firmware to the target (boot loader).

 

This works on the M5223X and M5225X chips and can be completely tested in the uTaster simulator.

 

Regards

 

Mark

 

www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

 

 

0 项奖励
回复