MCF5485 FEC design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5485 FEC design

1,778件の閲覧回数
Jason_Shi
Contributor I

Because we need two ethernet on the design, so we change the MCF5482 to MCF5485, there are two ethernet PHYs needed for the FEC. Are there more cheaper solution? fg. just one ethernet PHYs?

 

your suggestion is appreciative

 

Thank you again

ラベル(1)
0 件の賞賛
返信
1 返信

1,091件の閲覧回数
JWW
Contributor V

Jason,

 

You can buy ethernet phys that are "dual-phy" capable.  You can then connect two FEC channels to the single chip and then two sets of magnetics and jacks...

 

Take a look at the MCF54455 page.  The EVB board for this V4 ColdFire has two FECs and uses a dual-phy example with RMII.  You should be able to reference this evb board design.

 

Board name is: M54455EVB

 

-JWW

 

0 件の賞賛
返信