MCF5445x running code from internal SRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF5445x running code from internal SRAM

1,824 次查看
M_H_
Contributor I
Hi,
 
Has anyone been able to run code in the internal SRAM of the MCF5445x processor without enabling back-door access? If you have, how did you do it?
 
I can run code if the back-door is enabled but according to the device errata you shouldn't enable back-door and core access at the same time. When I only enable the back-door my code runs about 40% slower which I assume is because back-door access is slower than core access and my stack is in the SRAM. If I don't enable back-door access then the processor resets as soon as a function is called that sits in the SRAM. I can read and write data (and the stack) when only core access is enabled but can't run code.
 
Thanks.
 
Malcolm
标签 (1)
0 项奖励
回复
1 回复

1,212 次查看
M_H_
Contributor I
So far I've learnt that there is an error in the manual regarding the internal SRAM but I have not found out what the solution is.
 
I believe it is only possible to have either code or data in the SRAM but not both when connected directly to the core.
 
It's about time a new manual was released for this processor since there are so many errors in the existing one (Rev 2) or at the very least an updated list of errata.
0 项奖励
回复