MCF54455 Serial Boot Facility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF54455 Serial Boot Facility

1,312 Views
IanW
Contributor I

The manual, MCF54455RM, states that, during the serial boot load, the SRAM base address is set to 0. The SRAM section says that the base address has to be in the range 0x80000000 to 0x8FFF8000.

What's going on?

Labels (1)
0 Kudos
Reply
1 Reply

996 Views
TomE
Specialist II

Section "12.4.3 Execution Transfer" of the Reference Manual is going on.

 

4. The actual memory that responds to the reset vector fetch depends on whether serial boot load is
   requested:
   — If SBFSR[BLL] is cleared, the reset vector fetch is handled by the FlexBus module, and
      whatever external memory is mapped at address 0, governed by the user-provided setting of
      RCON/CCR[FBCONFIG].
   — If SBFSR[BLL] is set, the reset vector and boot code are read from the on-chip SRAM. (The
      SBF enables the SRAM and maps it to address 0 via the RAMBAR before control of the
      processor is restored to the ColdFire core.) The reset vector (initial stack pointer and program
      counter) should point to locations in the on-chip SRAM,

0 Kudos
Reply