MCF54415 External Flash.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF54415 External Flash.

Jump to solution
4,800 Views
Skankanala
Contributor I

Hello,

I am looking for an example Firmware for MCF54415 that uses CS0 pin within Flexbus to access External Flash(16 bits 4MB). Secondly, I have to copy the data from FLASH to Internal SDRAM. Any suggestion/help is appreciated.

Thanks

0 Kudos
Reply
1 Solution
4,784 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer attached MCF54418 product validation code.

Related Flexbus and SDRAM module initialization code located at <sysinit.c> file.

Wish it helps.

Mike

View solution in original post

0 Kudos
Reply
3 Replies
4,776 Views
Skankanala
Contributor I

Thank you for the code Mike. Does NXP provide an Eval board to debug and test with the above Firmware ?

 

Sai.

0 Kudos
Reply
4,760 Views
TomE
Specialist II

> Does NXP provide an Eval board to debug and test with the above Firmware ?

Ten years ago, yes.

https://www.nxp.com/products/no-longer-manufactured/coldfire-mcf5441x-tower-system-module:TWR-MCF544...

It was available from the usual sources, but is now "obsolete":

https://www.arrow.com/en/products/twr-mcf5441x-kit/nxp-semiconductors

Development boards are only available when a device is new, as that's when everybody starts developing with it.

The following page has a graph on it showing the development board went from EOL to Obsolete half way through 2013:

https://ciiva.com/part/twr-mcf5441x-3761889

If you could get that board it wouldn't help. It plugs into a "TOWER" system, so you'd need the rest of that as well. Then all the tools are the same age and not very available.

Tom

 

0 Kudos
Reply
4,784 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer attached MCF54418 product validation code.

Related Flexbus and SDRAM module initialization code located at <sysinit.c> file.

Wish it helps.

Mike

0 Kudos
Reply