MCF5282 MAC radio reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF5282 MAC radio reset

1,702 Views
kj
Contributor I

Hello Forum members

I am using Coldfire MCF5282 EVB and trying to run 802.15.4 based application MyWirelessApp.

It compiles well but when I try to debug it gets stuck in radio reset in function MC1319xDrv_reset(void) at line while(!IrqContrilLib_IsMC1319xIrqAsserted()); this condition is always true.

 

and routine gets blocked there. Does anybody have also faced similar problem? Any help is highly appreciated.

Best Regards:
Santosh Dwivedi 
Labels (1)
0 Kudos
Reply
1 Reply

1,095 Views
kj
Contributor I
I sloved the problem. if you get stuck in such issue do following it helped to me.
1. use CW 6.4
2. Check RxTxEnable, Reset, SPI, ATTN , SwitchAntena pin  configuiratio
 
0 Kudos
Reply