MCF5272 - timer tin0 and tin1 input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5272 - timer tin0 and tin1 input

1,304件の閲覧回数
phanirajnarahar
Contributor I

I had made a small circuit with micro controller to generate pulses from 1 and 10 pulses per second. When circuit generates 1 pulse per second, it shall generate maximum of 10 pulses (i.e it shall generate for 10 seconds) and similarly when circuit generates 10 pulses per second and it shall generate the maximum of 500 pulses(i.e for 50 seconds). The result capturing is show in below table.

 

 

Header 1Header 2Header 3
HzF1 - (tin0 input)Total Count
12-426
1023-241270

 

Please get me a solution on above problem.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,180件の閲覧回数
TomE
Specialist II

You're not going to get a response to something that reads like a "school project".

The specification is incomplete anyway. Nobody could follow what you've written.

Tom

0 件の賞賛
返信