MCF52233 Ethernet Autonegotiation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF52233 Ethernet Autonegotiation

1,789 次查看
IRTrans
Contributor III

Hi,

we are working on a project based on the MCF52233. We are using the FNET IP Stack.

 

We are already using our own HW. Everything ist working fine, however the Ethernet Autonegotiation does not work correctly. We do get a link but only 10MBit  / Half Duplex. The "Auto-Negotiation Complete bit" (ACOMP) in the MII Status register is never set. Nevertheless a 10MBit Half Duplex connection is established. With manual parameters we can get 100 MBit FDX.

 

Apart from the FNET code I have tried the PHY init code used in the Coldfire TCP Lite stack, however the problem is the same.

 

We are using a MCF52233 with mask version 3M23E - this version is no longer affected by the common Autonegotiation bug.

 

Does anybody have working code for the Autonegotiation?

Has anybody used Autonegotiation on the MCF52233/52235 at all?

 

Thanks in advance, Marcus

标签 (1)
0 项奖励
回复
2 回复数

1,610 次查看
butok
NXP Employee
NXP Employee

Hi Marcus,

>>We are using a MCF52233 with mask version 3M23E -

>> this version is no longer affected by the common Autonegotiation bug.

How do you know that it is not affected by the auto-negotiation bug? Do you have a test code that can prove it?

Thanks,

Andrey

0 项奖励
回复

1,610 次查看
IRTrans
Contributor III

At least the Errata says the the 3M23E mask version is no longer affected by the bug ...

Marcus

0 项奖励
回复