MCF52223 looking for an example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52223 looking for an example

5,756件の閲覧回数
martin_schaffne
Contributor I
Hi
I am doing a dissertation submitted for a
diploma about implementing USB- Host in an
embedded system. I have chosen the MCF52223 microcontroller.
But I have no idea where to start, so I ask
you... is there any example code that could help me understand a little bit?
The application I am thinking at is standalone
without need of an OS. I should be able to
read/write on an USB- memorystick.

Thanks a lot
M. Schaffner
ラベル(1)
0 件の賞賛
返信
7 返答(返信)

2,994件の閲覧回数
martin_schaffne
Contributor I
Thanks for helping me.

cu
M. Schaffner
0 件の賞賛
返信

2,994件の閲覧回数
PopsStack
Contributor I
I have downloaded this file - can someone please advise how to implement this on the 52223EVB. Am I correct in sayting that this forms the basis of code required for Mass Class Storage for the EVB platform as the host and file transfer to and from the Mem stick.
 
Many thanks
 
Nic
 
0 件の賞賛
返信

2,994件の閲覧回数
DrSeuss
Contributor I
The attached will release to the 5222x product page Monday.
 
Message Edited by t.dowe on 2009-09-02 05:01 PM
0 件の賞賛
返信

2,994件の閲覧回数
cu202
Contributor I
Are there more examples on the MCF52223 since the last post in this forum? Looking for practical examples with useful explanation...
 
Thanks for any suggestion (links, codes et)..
0 件の賞賛
返信

2,994件の閲覧回数
martin_schaffne
Contributor I
Thanks for the information.
Could you pleas post the link when it is
available ?

Can I ask you from where this information
comes from ?

Regards
-M-
0 件の賞賛
返信

2,994件の閲覧回数
DrSeuss
Contributor I
Host side software should post this week.
HID (joystick,mouse,and keyboard) as well as Mass storage examples are included.
0 件の賞賛
返信

2,994件の閲覧回数
mjbcswitzerland
Specialist V
Hi M. Schaffner

Freescale has a beta of the ColdFire MCF5222X USB Device Mode Stack at the following address:

https://www.freescale.com/webapp/sps/download/license.jsp?colCode=MCF5222X_USB_DEVICE_BETA&nodeId=01...

You can download it as long as you accept the Freescale Semiconductor Software License Agreement and are registered.

Regards

Mark Butcher
www.mjbc.ch / www.uTasker.com
0 件の賞賛
返信