MCF5221X debugger / programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF5221X debugger / programmer

1,484 Views
gaminn
Contributor IV

Hello,

I bought this TBLCF board http://www.cncgeeker.com/index.php?main_page=product_info&cPath=7_4&products_id=9&zenid=092a0a87458f... and I would like to program my MCF52213 MCU. As far as now I noticed that my MCU is not in the supported list of the board.

 

I tried to use the debugger to program my MCU but no success. I can see some activity on DSI pin (two square waves) and DSCLK pin (clocks, 120 kHz approx.) when I push Debug button in CodeWarrior IDE (v 7.2). But no activity on DSO pin. I get "can't connect" message in CodeWarrior. The MCU is powered by 3.3 V.

 

 Is there anyone who uses TBLCF together with MCF5221X and can give me some suggestion how to fix my problem?

 

Thank you

 

Martin

Labels (1)
0 Kudos
Reply
1 Reply

1,199 Views
TomE
Specialist II

Read through to the end of the "TBLCF-open-source-debugging-cable" thread that is anchored to the top of this forum.

 

0 Kudos
Reply