MCF5216CVF66  - I do not see a decoder in the datasheet telling me the difference between MCF5216CVF66 and MCF5216CVM66

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF5216CVF66  - I do not see a decoder in the datasheet telling me the difference between MCF5216CVF66 and MCF5216CVM66

1,372件の閲覧回数
davidriness
Contributor I

Customer has an existing design, and needs to know if they can swap one for the other

 

Thank you

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,184件の閲覧回数
TomE
Specialist II

It isn't in the Data Sheet.

This is a PACKAGING difference:

32-bit microcontroller with CAN|NXP

As far as I can tell from this limited information, "CVM" is Lead Free and "CVF" isn't.

So it might affect your production in that there may be soldering problems changing from one package to the other.

Tom

0 件の賞賛
返信