MCF51QE/ I2C question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF51QE/ I2C question

1,721 次查看
mlun
Contributor I

Hello,

I am going to use the IIC-module on a MCF51QE32 and I was reading the in the reference manual page 267, about generating a start signal:  

Master Mode Select. The MST bit changes from a 0 to a 1 when a start signal is generated on the bus and master

mode is selected.

I dont understand this.. Shouldnt it be something like this:

Master Mode Select. When the MST bit changes from a 0 to a 1  a start signal is generated on the bus and master mode is selected.

 

Regards

 

Magnus

 

标签 (1)
0 项奖励
回复
2 回复数

1,302 次查看
mlun
Contributor I

Another question..

When I simulate using IIC2-module, I get the message "IIC2 module not implemented".

Device is MCF51QE32 and CW V6.3.  As far as I can understand the IIC2-module should be implemented in the device, but can the simulator only handle one IIC-module?

 

/Magnus

0 项奖励
回复

1,302 次查看
mlun
Contributor I

I replaced IIC2 with IIC1 and still get the message IIC1-module not implemented, so I guess this is just a simulator problem..

 

Magnus

0 项奖励
回复