MCF51

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51

2,312 Views
SecondTechCo
Contributor IV

Has anyone migrated from an MCF51 project ot a kinetis.  How hard is the project.  In looking for something closely compatible.  Is this the right route ?  MY processor is at its longevity

Labels (1)
0 Kudos
Reply
1 Reply

2,228 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

NXP launched MCUXpresso SDK software package for Kinetis product, which provides lots of example demo for module driver and application example. Customer could refer those example projects as quick start the Kinetis product design.

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply