MC68F375

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC68F375

2,149 次查看
djjd
Contributor I

I have a chip:MC68F375BGMZP33.What is its IDE and version of codewarrior? please.

标记 (1)
0 项奖励
回复
3 回复数

1,982 次查看
miduo
NXP Employee
NXP Employee

Hi,

Part MC68F375 is quite old and we do not have much resource to support it. For the IDE, you may use the CodeWarrior for 68K, which can been download here:

CodeWarrior® Development Tools for 68K|NXP 

0 项奖励
回复

1,982 次查看
TomE
Specialist II

I can see the original poster's confusion.

He has an MC68F375.

Currently available products here in this range consist of:

MC68000, MC68302, MC68331, MC68332, MC68340, MC68360, MC68F375.

The ones supported by CodeWarrior on that link consists of:

MC68302, MC68306, MC68331, MC68332, MC68340, MC68360.

ColdFire® Microcontrollers|NXP 

CodeWarrior® Development Tools for 68K|NXP 

It may be there's a mistake on the CodeWarrior page, and it does support the MC68F375 "out of the box". If it doesn't then there may need to be "some assembly required" in order to define an appropriate set of header files to suit the peripherals on that specific CPU model.

DJJ, do you have the debug pod hardware there for this chip? If not, then getting one might be the next challenge.

Tom

0 项奖励
回复

1,982 次查看
miduo
NXP Employee
NXP Employee

Hi, Tom

Yes, the CodeWarrior page is mistake. The MC68F375 is supported by CodeWarrior for 68K. From what I know the PROG32Z also support the MC68F375, see detail here:

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 
0 项奖励
回复