M52235EVB Exception vector name: Address Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52235EVB Exception vector name: Address Error

5,177件の閲覧回数
Evan_Chn
Contributor I
When I run the DEMO project TCPIP stack on the M52235EVB board ,I got a message "Exception vector name:Address Error" in mcf5223_lo.s on the line:move.1 #__SRAM,d0,what's wrong ?
thanks
ラベル(1)
0 件の賞賛
返信
6 返答(返信)

2,610件の閲覧回数
DrSeuss
Contributor I
It would appear that you have not programmed the code into the device. Use that CW flash programming tool on the title bar. Please see:

http://www.freescale.com/coldfireseminars

for a walk though.

 

Alban corrected link

Message Edited by Alban on 2007-02-09 11:27 AM

0 件の賞賛
返信

2,610件の閲覧回数
Evan_Chn
Contributor I
thanks.After I programmed it into the flash with CF Flasher,it runs with no errors 
0 件の賞賛
返信

2,610件の閲覧回数
Ale
Contributor I
I have the same problem, but the link previously postend don't work!
 
Can I have a new link??
 
 
0 件の賞賛
返信

2,610件の閲覧回数
Alban
Senior Contributor II
Hello,
 
I have corrected the link in the previous post.
it was Cold and not Code in the URL :smileywink:
 
Cheers,
Alban.
0 件の賞賛
返信

2,610件の閲覧回数
Ale
Contributor I
Thanks, it works fine!!!!
0 件の賞賛
返信

2,610件の閲覧回数
Nouchi
Senior Contributor II
0 件の賞賛
返信