Looking for Simple TCP/IP Example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for Simple TCP/IP Example

2,502 Views
SBS
Contributor I
Hi,
 
I am looking for a simple TCP/IP example.  All I want to do is send messages down to my ColdFire ethernet device.
 
For example, I have a simple program I wrote that I can put on two computers and send text strings between them using TCP.  This is basically what I want to do with the ColdFire microcontroller. 
 
Is there a simple example out there that does this?
 
Thanks,
Sal
Labels (1)
0 Kudos
Reply
2 Replies

1,634 Views
net11
Contributor III

If someone has any examples on this, it would help me too !

0 Kudos
Reply

1,634 Views
MCF52233
Contributor III

Hi , why don't you look for coldfire-lite.

It contains lots of example.

 

Thanks and Regards,

Abhijit Khadtare

0 Kudos
Reply