LS1021ATSN-PA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021ATSN-PA

1,662 Views
s180101037
Contributor I

根据教程将sdcard.img编程到sd卡中之后,我将sd卡插入板中,加电,然后使用pc将其连接到板中。我发现我的PC无法识别串行端口。

Tags (1)
0 Kudos
Reply
1 Reply

1,544 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Sorry for your post the QorIQ question at ColdFire sub-forum.

Could you please move this thread to QorIQ sub-forum?

If you couldn't, Could you post the same question thread at QorIQ sub-forum?

https://community.nxp.com/community/qoriq?tid=community 

Thanks for the understanding.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply