KSZ8041 PHY Chip for the MCF52259

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KSZ8041 PHY Chip for the MCF52259

4,613 次查看
ND
Contributor I
Hi,
   I have on order MCF52259 processors and also ordered KSZ8041 PHY as in the demo kit.  The demo kit has the KSZ8041NL , but I can only get the KSZ8041TLI part. The only difference I can see is that the TLI part also does SMII interface, package type, and about £1 more expensive. I have never used a PHY chip before, but can anyone tell me if there would be a problem using this one?

Thanks
Neil
标签 (1)
0 项奖励
回复
4 回复数

2,249 次查看
HLaidet
Contributor I

Hello,

 

I used a KSZ8041TL connected to a MCF52259 because TQFP package is easier to solder.

It runs with the same software the DEMO board.

 

The only problem i had (lost link sometimes) was the capacitors on quartz too low (18pF increased to 33pF).

 

No other problems.

 

Regards,

 

Henri

 

0 项奖励
回复

2,249 次查看
Flaviohpo
Contributor II

what do you mean with:


"The only problem i had (lost link sometimes) was the capacitors on quartz too low (18pF increased to 33pF)."

 

did u use an independent crystal for the CI? whats frequency? 25MHz?

0 项奖励
回复

2,249 次查看
HLaidet
Contributor I

i use the basic schematic with a crystal 25MHz(Fundamental)+1M resistor and two 18pF capacitors ( like the schematic of M52259DEMO board ).


the quartz is: CITIZEN HCM49 25.000MABJ-UT

 

because it is the first time i use a PHY, then i did a test endurance.

 

that's when i found errors ethernet.

 

by putting traps, i have found losses of LINK (status register, bit LINK STATUS).

to get everything correct, i had to increase the 18pF capacitors on quartz.


now the test is done without errors (several hours).

 

Henri

 

0 项奖励
回复

2,249 次查看
Flaviohpo
Contributor II
I have the same question, but I also would like to know some alternatives to the KSZ8041NL that is not QFN package. Thanks.
0 项奖励
回复