JM Badge Board Trouble

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

JM Badge Board Trouble

跳至解决方案
1,158 次查看
Kiwi
Contributor I

Hi,

just got the Flexis JM Badge Board. Connecting it to my Win7 machine has it shown in the Device Manager as a HID Keyboard device and also under Human interface Devices as a USB input device. I have tried to manually update the driver from the Windows7SensorDevKit->Drivers->Binaries->AMD64->SensorBadgeDriver but it fails.

There is another post that describes connecting the board via USB, then hitting E8 twice (http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=7930&query.id=173070#...) , but this totally freaked out my computer.

 

So I am stuck, all the preloaded demos work. Pluggin in via usb then hitting E5 and then E8 allow me to use the touch sensors as buzzer notes. Besides that I got nothing.

 

Any help would be most appreciated,

Kind regards,

Kiwi

标签 (1)
0 项奖励
回复
1 解答
488 次查看
mnorman
NXP Employee
NXP Employee

Hi, Kiwi,

 

Can you get the USB bootloader mode (mass storage device) to enumerate correctly? 

 

Does this post help?

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=7930#M7930

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
489 次查看
mnorman
NXP Employee
NXP Employee

Hi, Kiwi,

 

Can you get the USB bootloader mode (mass storage device) to enumerate correctly? 

 

Does this post help?

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=7930#M7930

 

0 项奖励
回复
488 次查看
Kiwi
Contributor I

Hi MNorman,

you know I had actually read that post, but didn't get it. So you pointing me back to it, a fresh day, and all is good. My many thanks for such a speedy reply. The board is simply brilliant. Everything I hoped it would be having watched the PDC videos of it.

 

Cheers,

Kiwi

0 项奖励
回复