IP cores

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IP cores

4,791 Views
garimella
Contributor I

I have found free  IP cores for 68k processors on the web. Can we use those cores in commercial applications as a substitute for legacy 68k processor(s)? What are the legal implications?Does NXP/motorola still hold patent rights for 68k family(68000,68010, 68020 and so on)?

0 Kudos
Reply
5 Replies

4,774 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer the webpage [IP-block Licensing], there listed 68K core IP.

NXP is licensing many functional IP blocks in various fields. An IP block is a reusable unit of logic, cell, or chip layout design and can be used as building block for various chip- and logic designs. By making this technology available NXP is opening up the opportunity for chip designers to leverage our world-class building blocks in a wide assortment of on-chip solutions. Several IP block licenses include relevant application software.

Please contact with your local NXP distributor about IP licensing.Thanks.

best regards,

Mike 

0 Kudos
Reply

4,748 Views
TomE
Specialist II

> there listed 68K core IP.

Where exactly? That page lists:

  • CoolFlux DSP Family
  • MIPI I3C
  • USB 2.0 Full High Speed Solution
  • FLEXRAY Communication Controllers
  • FlexCAN Controller
  • e200 Core Family, NXP Power Architecture™ IP
  • StarCore DSP
  • Coldfire 32-Bit Processors

There are no 68000 (or 68020 or 68300 or CPU32) cores listed there.

The 68000 (being asked about) CPUs are so old they were probably hand-taped, so I wouldn't expect NXP to have IP that would fit in an FPGA for them.

Tom

 

0 Kudos
Reply

4,737 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Tom,

You are right. The [IP-block Licensing] program does not include 68K core.

68K core is quite old and I need to check with internal team about 68K core IP info.

Thank you all for the patience.

best regards,

Mike

0 Kudos
Reply

1,645 Views
wenuam
Contributor I

Hello, any news about the status of 68k IP cores' right ?

0 Kudos
Reply

4,770 Views
garimella
Contributor I

I am looking for legal implications if we were to use rasberry Pi based emulator for 68k processor. Please clarify as buying new IP core is out of question.

0 Kudos
Reply