I need Help about DEMOEM MCF51EM256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need Help about DEMOEM MCF51EM256

1,408 Views
andrxs
Contributor I

Hello

 

I have a little problem with targert DAMOEM, it's used MCF51EM256 microcontroller, I'm trying to programmer with the example Freescale give, all go so fine I programmed, but when I want to run the example the targert not show nothing, I think that it could be the clock configurated, but I don't know I try too the MCU show me something in Hyperterminal but I tasted the signals and show so fine in oscilocopy, but in the hyperterminal don't show nothing, Somebody could help me with this problem?... 

 

Thaks

Labels (1)
0 Kudos
Reply
1 Reply

1,051 Views
JWW
Contributor V

Andrxs,

 

If you could provide a bit more detail, then I'm sure others on the forum could help a bit.

 

If you could provide the specific demo and status of any LEDs etc on your board.  Also, which devtool you are using etc...

 

Hope this helps

JWW

 

0 Kudos
Reply