I need Help about DEMOEM MCF51EM256

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I need Help about DEMOEM MCF51EM256

1,391件の閲覧回数
andrxs
Contributor I

Hello

 

I have a little problem with targert DAMOEM, it's used MCF51EM256 microcontroller, I'm trying to programmer with the example Freescale give, all go so fine I programmed, but when I want to run the example the targert not show nothing, I think that it could be the clock configurated, but I don't know I try too the MCU show me something in Hyperterminal but I tasted the signals and show so fine in oscilocopy, but in the hyperterminal don't show nothing, Somebody could help me with this problem?... 

 

Thaks

ラベル(1)
0 件の賞賛
返信
1 返信

1,034件の閲覧回数
JWW
Contributor V

Andrxs,

 

If you could provide a bit more detail, then I'm sure others on the forum could help a bit.

 

If you could provide the specific demo and status of any LEDs etc on your board.  Also, which devtool you are using etc...

 

Hope this helps

JWW

 

0 件の賞賛
返信