I'm using the TWR-MECH board that has the 3-axis accelerometer. Help finding programming information.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I'm using the TWR-MECH board that has the 3-axis accelerometer. Help finding programming information.

1,762 Views
jamil_faulkner
Contributor I

Is there any information on the daughter card that is used for the MMA7455 accelerometer? The daughter card is labeled as LFDA7455. I was able to find a schematic but I was looking for more info that would be helpful for me programming the board. Any guidance in the right direction would be helpful, thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,621 Views
DavidS
NXP Employee
NXP Employee

Hi Jamil,

If you go to the Tower Product page for this board there is a link to download the CodeWarrior Sample Code for it:

Product Page:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-MECH

Current Updates and Releases

· TWR_MECH_FSLBOT_CW_SC<http://cache.freescale.com/files/sensors/software_tools/TWR_MECH_FSLBOT_CW_Sample_Code.zip?fpsp=1>: CodeWarrior Sample Code.

Note that it is a bit old.

Regards,

David

0 Kudos
Reply