I'm using the TWR-MECH board that has the 3-axis accelerometer. Help finding programming information.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I'm using the TWR-MECH board that has the 3-axis accelerometer. Help finding programming information.

1,753件の閲覧回数
jamil_faulkner
Contributor I

Is there any information on the daughter card that is used for the MMA7455 accelerometer? The daughter card is labeled as LFDA7455. I was able to find a schematic but I was looking for more info that would be helpful for me programming the board. Any guidance in the right direction would be helpful, thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,612件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Jamil,

If you go to the Tower Product page for this board there is a link to download the CodeWarrior Sample Code for it:

Product Page:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-MECH

Current Updates and Releases

· TWR_MECH_FSLBOT_CW_SC<http://cache.freescale.com/files/sensors/software_tools/TWR_MECH_FSLBOT_CW_Sample_Code.zip?fpsp=1>: CodeWarrior Sample Code.

Note that it is a bit old.

Regards,

David

0 件の賞賛
返信