How to send integer data using MOTUSB Host end driver to the device side(MCF5272)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to send integer data using MOTUSB Host end driver to the device side(MCF5272)

3,410 Views
AshwinBhamburka
Contributor I
Hello,
 
We are using the 'MOTUSB' driver for communication with MCF5272 processor.  We are facing some problem in adding the code to the MOTUSB driver.
Problem Statement:
We want to send an integer data using the exsisting functions in motusb.lib, from the host to the device(MCF5272 processor). For this application, which function is best suitable and which parameter/s of the function can be used for this?
OR
Does anyone have the code for motusb.lib ?
 
Any suggestions on this implementation are welcome.
 
Regards
Ashwin.
Labels (1)
0 Kudos
Reply
2 Replies

1,900 Views
AshwinBhamburka
Contributor I
Hello Andrey Butok,
 
Thanks for the help.
 
We got the source from the freescale web-site. We are now searching if we can get the '*.lib' (library) files. So that we can modify/customise the USB Host utility to suit to our application.
 
Your suggestions are welcome.
 
Regards,
Ashwin.
0 Kudos
Reply

1,900 Views
butok
NXP Employee
NXP Employee
Hi Ashwin
 
 
You must be lucky  - I found your message and I have the copy of source codes (attached) it's abot 5 years old...
Please do no ask about additional support - you have source codes, and the guy who developed it is not available now.
 
Best regards
Andrey Butok
Message Edited by t.dowe on 2009-10-21 02:11 AM
0 Kudos
Reply