How to connect a Wlfson codec WM8750 to MCF5251 CPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to connect a Wlfson codec WM8750 to MCF5251 CPU

2,815件の閲覧回数
Varindra
Contributor I
Hi,
         We have to interface the WM8750 codec to MCF5251, this CPU has 3 no. I2S
Controller - 1st Interface is I/O, 2nd interface is only Out & 3rd
interface is only In. We are not sure about the status about the  DAC &
ADC (Word Clock) in the WM8750 codec, i.e. whether there are two seperate clock
required while bit clock can be the same. Presently we have taken word clock
from 1st interface & 2nd interface, bit clock from the 1st interface and
DIN & DOUT from the 1st interface of the MCF5251 to WM8750 codec connection. Is
it ok ? or else how we can connect.

WM8750 has a common bit clock, ADCLRC & DACLRC (i.e. seperate word clock for ADC &
DAC inside), DIN, DOUT.

Thanks & Regards,
Varindra
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,555件の閲覧回数
ShenLi
Contributor I
Hello, Varindra
I am doing a M5253 design with WM8731, I think it might give you some help. Please check the attachment. I have successfully run  a simple loop back (from earmic to earphone) through WM8731+ MCF5253.
0 件の賞賛
返信

1,555件の閲覧回数
Varindra
Contributor I
Hi Shen,
                  Thanks for the reference.

Thanks & Regards,
Varindra
0 件の賞賛
返信