Flashing a MCF52233 in-system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing a MCF52233 in-system

1,650件の閲覧回数
ZeroOne
Contributor I
Hello

I have a M52233DEMO board and I am considering to create my own board for a project I have in mind.
Is it possible to flash a new board with a MCF52233 onbord, in-system so to speak?

If yes, how?

Regards

Kim

ラベル(1)
0 件の賞賛
返信
1 返信

987件の閲覧回数
mjbcswitzerland
Specialist V
Hi

See the following: http://www.utasker.com/forum/index.php?topic=77.0

If you only want to FLASH programs (and not debug) the EZport offers the simplest connection - code running on the M52233DEMO can also do this - see: http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=3911&query.id=30163#M...

Regards

Mark

0 件の賞賛
返信