Failed to Open. Plug DEMO board into PC via USB cable.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to Open. Plug DEMO board into PC via USB cable.

1,499件の閲覧回数
rodrigocorrêa
Contributor II

Hello.
I'm having trouble to connect my DEMOEM board to the computer through the Terminal Utility.

 

I'm using the DEMOEM board for COLDFIRE MCF51EM256. I can download a program to the broard, written in the CodeWorrior 6.3 and debug it; All drivers seems to be correctly installed: in the device manger, I can see the Jungo Connectivity and PEMicro USB ans Serial interface (i00) and (i01); I am using Windows 10.

 

Can anybody help me?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,303件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

What is your setting of the Terminal Utility? There should have no hardware issue because you had connect the board success, so it is really an software issue.

0 件の賞賛
返信